SNIS217C december 2020 – may 2023 TMP139
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
When the SETAASA CCC is issued by the host controller to the TMP139, it shall switch from I2C mode to I3C basic mode. The CCC takes effect after a Stop has been issued by the host controller. Once the SETAASA is received, the TMP139 shall set the MR18 register bit INF_SEL as 1'b1 for I3C basic mode of operation.
The CCC is always issues as a broadcast command, as shown in Figure 7-35, with no PEC bytes since it is applicable only during I2C mode.
TMP139 NACKs the SETAASA CCC if the previous CCC transaction has a parity error and the host starts the transaction with a Repeated Start.