SNIS217C december 2020 – may 2023 TMP139
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The DISEC CCC is issued by the host controller to disable the event interrupt generation. The CCC takes effect after a Stop has been issued by the host controller. Once the DISEC is received, the TMP139 shall the update MR27 register bit IBI_ERROR_EN to 1'b0.
It is illegal for the host controller to send the DISINT bit as 0.
The command may be issued either as a broadcast command or as a direct command to a specific device as shown in Figure 7-29 and Figure 7-30.
The command may be issued either as a broadcast or as a direct command, as shown in Figure 7-31 and Figure 7-32, with PEC Enabled. In such a case the host controller shall append the PEC byte calculated on all bytes except the byte with 7'h7E and R/W=0 after the Start or Repeated Start.
TMP139 NACKs the DISEC CCC if the previous transaction has a parity or PEC error and the host starts the transaction with a Repeated Start.