SBOSA45C february 2022 – may 2023 TMP1826
PRODUCTION DATA
The host can issue this command to select all the devices on the bus. This is useful when the host wants to write to the scratchpad-1 or trigger the temperature conversion for all the devices on the bus. Additionally, the host can use the command to increase the overall bus data throughput when there is a single device on the bus.
The host must take care to not issue the command when there are multiple devices on the bus,. If the host intended to read the devices with this command, it would cause a collision on the bus.