SBOSA45D February 2022 – January 2025 TMP1826
PRODUCTION DATA
Figure 8-22, Figure 8-23 and Figure 8-24 show the function phase that follows the address phase. The host can present different functions during this phase, which is followed by either the host sending data to the device, reading device data, or starting a temperature conversion. Some of the functions can be broadcast to all the devices on the bus using SKIPADDR or OVD SKIPADDR. Read functions must always be unicast with a device selected during the address phase using MATCHADDR, FLEXADDR or OVD MATCHADDR. For cases, where there is a single device on the bus, the device address selection can be skipped.