SBOSA45C february 2022 – may 2023 TMP1826
PRODUCTION DATA
Place the power-supply bypass capacitor as close as possible to the supply and ground pins when in supply powered mode (see Figure 10-4). The recommended value of the capacitor is 0.1 µF. The open-drain SDQ pin requires an external pullup resistor which must not be higher than RPUR.
When in bus powered mode, only the external pullup resistor is required for the open-drain SDQ pin. As shown in Figure 10-5, TI recommends to place a 20-KΩ pullup resistor when connecting IO to SDQ pin to avoid shorting the SDQ to GND in case the IO is configured as an output and driven low (see Figure 10-6). The ADDR pin resistor uses very low current to decode the short address and should be placed close to the device, if possible. Take care to avoid leakage currents to prevent incorrect decoding.