SBOSA45C february 2022 – may 2023 TMP1826
PRODUCTION DATA
The temperature alert feature uses the temperature alert low registers for low threshold comparison and temperature alert high registers for high threshold comparison. The format of the register is the same as the temperature results.
The device shall compare the result of the last conversion with the alert thresholds. If the temperature result is less than the low limit, or more than the high limits, then the device shall set the appropriate alert status flag, in the status register. The alert status flags are cleared based on the ALERT_MODE setting in the device configuration-1 register.
Additionally, if the IO2/ALERT pin is configured as an alert pin, the alert status is reflected on the pin in supply powered mode.