SBOSA45C february 2022 – may 2023 TMP1826
PRODUCTION DATA
To leverage the features effectively, the device access consists of three distinct phases. As shown in Figure 9-19, any bus communication starts with a bus reset condition to which every device on the bus must respond. This is followed by a highly configurable address phase, where the host selects the device it wants to access. Finally, there is a function phase where the host provides the selected device(s) the action it wants to take.
In a 1-Wire bus, all write and reads are initiated by the host except for the answer to reset which is initiated by the devices on the bus.