SBOSA45C february 2022 – may 2023 TMP1826
PRODUCTION DATA
The function is issued by the host to read the temperature result, status bits, and functional registers from the register scratchpad. The selected device transmits the first 8 bytes of the register scratchpad followed by CRC of the 8 bytes. If the host wants to continue the read operation, the host will receive the next 8 bytes along with CRC for the last 8 bytes. The host can terminate the function at any point by issuing a bus reset.