SBOSA45D February 2022 – January 2025 TMP1826
PRODUCTION DATA
The resistor address modes uses E96-series (1% tolerance) standard resistor connected between the ADDR pin and ground. Figure 8-6 shows the 8-bit address with the lower 4 bits decoded from the resistor connected, which is overlaid on the contents of the short address register.
After having FLEX_ADDR_MODE as '00b', the host controller must set the bits as '10b' in the device configuration-2 register which enables the device to decode the resistor connected. After writing the device configuration-2 register, the host must place the device in shut down mode and idle the bus for tRESDET, for the device to decode the resistor address. Table 8-3 shows the set value of the device address based on the decoded resistor value. If the ADDR pin connected to GND or lower than 6.49 kΩ, then the address decoder shall always decode as '0000b'. Similarly, if the ADDR pin is connected to a resistor higher than 54.9 kΩ, the address decoder shall always decode as '1111b'.
RESISTOR VALUE (kΩ) | ADDRESS DECODE |
---|---|
< 6.49 | 0h |
7.87 | 1h |
9.31 | 2h |
11.0 | 3h |
13.3 | 4h |
15.4 | 5h |
17.8 | 6h |
20.5 | 7h |
23.7 | 8h |
26.7 | 9h |
30.1 | Ah |
33.2 | Bh |
37.4 | Ch |
42.2 | Dh |
47.5 | Eh |
> 54.9 or floating | Fh |
This mode is useful when the application requires placing the TMP1826 on multiple printed circuit boards (PCBs). The Bill of Materials (BOM) component can be changed easily instead of having multiple PCBs fabricated for individual pin connections, thereby reducing the cost of the system.