SBOSA15B September 2022 – January 2025 TMP1827
PRODUCTION DATA
The host issues the command to access a device by the short address that is configured in the short address register. Using the command does not affect the 64-bit unique address of the device. The FLEXADDR command is followed by one byte, which is the short address of the device, the host wants to select for further communication.