SBOSA15B September 2022 – January 2025 TMP1827
PRODUCTION DATA
A host read is the means by which the hosts gets the data from the device or the CRC for data integrity check. A host read starts by the host driving the data line low as shown in Figure 8-11. When the device detects the falling edge, the device can drive the line low before the time tRL. The host can release the bus from the side after the time tRL(MIN) elapses. If the device intends to transmit a logic '1', then the bus is released before tRL(MAX) elapses. If the device intends to transmit a logic '0', then the bus is released after tSLOT(MIN). The host must sample the line after the time tRWAIT, for a time frame indicated by tMSW. The host must factor the rise time due to the pullup resistor and bus capacitance to determine the sampling window for the host to sample the bit level sent by the device or to drive the next read bit time slot.