SBOSA15B September 2022 – January 2025 TMP1827
PRODUCTION DATA
The auto conversion mode is a programmable feature in bus powered mode that can be enabled by setting the CONV_MODE_SEL as '10b' in the device configuration-1 register. As shown in Figure 8-14, the host can skip the issue of the temperature conversion request and directly read the temperature data from the device when the auto conversion mode is enabled. This enables the application to speed up the temperature conversion and read, because the request command is no longer required. As in the case for multiple device bus, a low impedance current path is required to meet the current requirement of the bus during the active conversions.