SBOSA15A september 2022 – may 2023 TMP1827
PRODUCTION DATA
The temperature offset has the same format as the temperature result and is stored in the temperature offset registers.
The device, after every temperature conversion, applies the offset value before the temperature is stored in the temperature result register. The host write to the offset register can be stored in the configuration EEPROM of the device, which removes the overhead for the host to reprogram the value or reapply in software at every power up. The offset features allow the device to achieve better accuracy at the temperature range for the application by performing a single point calibration.