SBOSA15B September 2022 – January 2025 TMP1827
PRODUCTION DATA
The function is issued by the host to read the temperature result, status bits, and functional registers from the register scratchpad. The selected device transmits the first 8 bytes of the register scratchpad followed by CRC of the 8 bytes. If the host wants to continue the read operation, the host receives the next 8 bytes along with CRC for the last 8 bytes. The host can terminate the function at any point by issuing a bus reset.