SBOSA15B September 2022 – January 2025 TMP1827
PRODUCTION DATA
The host can issue this command to select all devices which support overdrive speed in a mixed speed bus. This is useful when the host wants to write to the scratchpad-1 or trigger the temperature conversion for all the devices on the bus that support overdrive speeds. Additionally, the host can use the command to increase the overall bus data throughput when there is a single device on the bus. When the command is issued, only devices that support overdrive mode shall set the internal OD flag as '1'.
The host must take care to not issue the command when there are multiple devices on the bus which support overdrive mode. A collision on the bus is caused if the host attempts to read the devices with this command.
If the host issues a standard mode bus reset at any time, all devices which have OD flag set as '1' shall clear the same and revert back to standard mode speed.