SBOSA15A september 2022 – may 2023 TMP1827
PRODUCTION DATA
A host write is the means by which the host sends the command, function, and data to the devices. A host write starts by the host driving the data line low as shown in Figure 9-10. If the host intends to transmit a logic '1', the line is released after tWR1L time. If the host intends to transmit a logic '0', the line is released after tWR0L. After releasing the data, the pullup resistor causes the line to become high till the beginning of the next time slot. The device samples the line after tRDV has elapsed from the falling edge, for a time frame indicated by tDSW. The host must factor the rise time due to the pullup resistor and bus capacitance to determine the release of the data line before the line is sampled by the device and the host drives the next write bit time slot.