SPRSP68B January 2023 – November 2023 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
PRODMIX
Refer to the PDF data sheet for device specific package drawings
The CAN module uses the IP known as DCAN. This document uses the names CAN and DCAN interchangeably to reference this peripheral.
The CAN module implements the following features:
For a CAN bit clock of 100 MHz, the smallest bit rate possible is 3.90625Kbps.
The accuracy of the on-chip oscillator is in the INTOSC Characteristics table. Depending on parameters such as the CAN bit timing settings, bit rate, bus length, and propagation delay, the accuracy of this oscillator may not meet the requirements of the CAN protocol. In this situation, an external clock source must be used.
Figure 6-63 shows the CAN block diagram.