SCDS463A June 2022 – March 2023 TMUX4051-Q1 , TMUX4052-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
When the EN pin of the TMUX405x-Q1 devices is pulled low, one of the switches is closed based on the state of the address or select pins. When the EN pin is pulled high, all the switches are in an open state regardless of the state of the address or select pins.
Unused logic control pins must be tied to GND or VDD to be certain that the device does not consume additional current as highlighted in Implications of Slow or Floating CMOS Inputs. Unused signal path inputs (Sx and Dx) should be connected to GND.