SCDS384A September 2018 – December 2018 TMUX6119
PRODUCTION DATA.
Bandwidth is defined as the range of frequencies that are attenuated by < 3 dB when the input is applied to the source pin of an on-channel, and the output is measured at the drain pin of the TMUX6119. Figure 27 shows the setup used to measure bandwidth of the mux. Use Equation 4 to compute the attenuation.