SCDS384A September 2018 – December 2018 TMUX6119
PRODUCTION DATA.
When the EN pin of the TMUX6119 is pulled high, one of the two switches is closed based on the state of the SEL pin. When the EN pin is pulled low, both switches remain open irrespective of the state of the SEL pin. The EN pin is weakly pull-down internally through a 6MΩ resistor, thereby setting each channel to the open state if the EN pin is not actively driven. The SEL pin is also weakly pulled-down through an internal 6Mohm resistor, allowing channel A (SA to D) to be selected by default when EN pin is driven high. Both the EN pin and the SEL pin can be connected to VDD (as high as 16.5 V).