SCDS384A September 2018 – December 2018 TMUX6119
PRODUCTION DATA.
The on-resistance of the TMUX6119 is the ohmic resistance across the source (SA or SB) and drain (D) pins of the device. The on-resistance varies with input voltage and supply voltage. The symbol RON is used to denote on-resistance. The measurement setup used to measure RON is shown in Figure 17. Voltage (V) and current (ICH) are measured using this setup, and RON is computed as shown in Equation 1: