SCDS384A September 2018 – December 2018 TMUX6119
PRODUCTION DATA.
Transition time is defined as the time taken by the output of the TMUX6119 to rise or fall to 90% of the transition after the digital address signal has fallen or risen to 50% of the transition. Figure 20 shows the setup used to measure transition time, denoted by the symbol tt.