SLOS474E August 2005 – March 2016 TPA2005D1-Q1
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
These typical connection diagrams highlight the required external components and system level connections for proper operation of the device in several popular use cases.
Each of these configurations can be realized using the Evaluation Modules (EVMs) for the device. These flexible modules allow full evaluation of the device in the most common modes of operation. Any design variation can be supported by TI through schematic and layout reviews. Visit http://e2e.ti.com for design assistance.
For this design example, use the parameters listed in Table 1
PARAMETER | EXAMPLE |
---|---|
Power Supply | 5 V |
Shutdown Input | High > 2 V |
Low < 0.8 V | |
Speaker | 8 Ω |
Figure 38 shows the TPA2005D1-Q1 typical schematic with differential inputs, and Figure 40 shows the TPA2005D1-Q1 device with differential inputs and input capacitors, and Figure 41 shows the TPA2005D1-Q1 device with single-ended inputs. Differential inputs should be used whenever possible, because the single-ended inputs are much more susceptible to noise.
REF DES | VALUE | EIA SIZE | MANUFACTURER | PART NUMBER |
---|---|---|---|---|
RI | 150 kΩ (±0.5%) | 0402 | Panasonic | ERJ2RHD154V |
CS | 1 μF (+22%, –80%) | 0402 | Murata | GRP155F50J105Z |
CI (1) | 3.3 nF (±10%) | 0201 | Murata | GRP033B10J332K |
The input resistors (RI) set the gain of the amplifier according to equation Equation 19.
Resistor matching is very important in fully differential amplifiers. The balance of the output on the reference voltage depends on matched ratios of the resistors. CMRR, PSRR, and cancellation of the second harmonic distortion diminish if resistor mismatch occurs. Therefore, it is recommended to use 1% tolerance resistors, or better, to keep the performance optimized. Matching is more important than overall tolerance. Resistor arrays with 1% matching can be used with a tolerance greater than 1%.
Place the input resistors very close to the TPA2005D1-Q1 to limit noise injection on the high-impedance nodes.
For optimal performance, the gain should be set to 2 V/V or lower. Lower gain allows the TPA2005D1-Q1 to operate at its best and keeps a high voltage at the input, making the inputs less susceptible to noise.
The TPA2005D1-Q1 is a high-performance class-D audio amplifier that requires adequate power-supply decoupling to ensure the efficiency is high and total harmonic distortion (THD) is low. For higher frequency transients, spikes, or digital hash on the line, a good low equivalent-series-resistance (ESR) ceramic capacitor, typically 1 μF, placed as close as possible to the device VDD lead, works best. Placing this decoupling capacitor close to the TPA2005D1-Q1 is very important for the efficiency of the class-D amplifier, because any resistance or inductance in the trace between the device and the capacitor can cause a loss in efficiency. For filtering lower-frequency noise signals, a 10-μF, or greater, capacitor placed near the audio power amplifier also helps, but it is not required in most applications because of the high PSRR of this device.
The TPA2005D1-Q1device does not require input coupling capacitors if the design uses a differential source that is biased from 0.5 V to VDD – 0.8 V (shown in Figure 38). If the input signal is not biased within the recommended common-mode input range, if needing to use the input as a high pass filter (shown in Figure 40), or if using a single-ended source (shown in Figure 41), input coupling capacitors are required.
The input capacitors and input resistors form a high-pass filter with the corner frequency, fc, determined in Equation 20.
The value of the input capacitor is important to consider, as it directly affects the bass (low frequency) performance of the circuit.
Equation 21 is reconfigured to solve for the input coupling capacitance.
If the corner frequency is within the audio band, the capacitors should have a tolerance of ±10% or better, because any mismatch in capacitance causes an impedance mismatch at frequencies lower than the corner frequency.
For a flat low-frequency response, use large input coupling capacitors (1 μF).