SLOS367E August 2003 – November 2015 TPA6211A1
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
Place all the external components close to the TPA6211A1 device. The input resistors need to be close to the device input pins so noise does not couple on the high impedance nodes between the input resistors and the input amplifier of the device. Placing the decoupling capacitors, CS and C(BYPASS), close to the TPA6211A1 device is important for the efficiency of the amplifier. Any resistance or inductance in the trace between the device and the capacitor can cause a loss in efficiency.