SCPS295 September 2024 TPLD801
ADVANCE INFORMATION
The TPLD801 has a power-on reset (POR) macro-cell to ensure correct device initialization and operation of all macro-cells in the device. The purpose of the POR circuit is to have consistent behavior and predictable results when the VCC power is first ramping to the device, and also while the VCC is falling during power-down. To accomplish this goal, the POR drives a defined sequence of internal events that trigger changes to the states of different macro-cells inside the device, and finally to the state of the I/O pins.
The power-on Reset (POR) macro-cell will produce a logic High signal as an output when the device power supply (VCC) rises to approximately VPORR and device completely starts up. All outputs are in high impedance state and chip starts loading data from OTP. The reset signal is released for internal macro-cells and all the registers are initialized to their default states. Figure 7-19 shows POR system generates a sequence of signals that enable certain macro-cells.
As shown in Figure 7-19, after the VCC has start ramping up and crosses the VPORR threshold:
Delay blocks will pass their inputs through to the output during the startup sequence without delaying the signal per the configuration, so a LUT added in front of the input of a DLY that ANDs the DLY input with POR will guarantee the input signal will not appear until the device has fully powered up.
GPIO quick charge: There is an option to connect a 2-kΩ resistor in parallel to any configured pull up/pull down resistors to help inputs get to the right voltage faster, especially if there is significant capacitance. The 10 kΩ, 100 kΩ and 1 MΩ GPIO pull up/pull down resistors are not enabled until the POR sequence is completed.
Initialization: All internal macro-cells are initialized to a low level by default. Starting from when VCC exceeds VPORR, macro-cells in the TPLD801 are powered on and forced into a reset state.
The POR signal going high indicates the mentioned power-up sequence is complete.