SLUSEZ3A December 2023 – December 2024 TPS1200-Q1
PRODUCTION DATA
For selecting the MOSFET Q1, important electrical parameters are the maximum continuous drain current ID, the maximum drain-to-source voltage VDS(MAX), the maximum drain-to-source voltage VGS(MAX), and the drain-to-source ON resistance RDSON.
The maximum continuous drain current, ID, rating must exceed the maximum continuous load current.
The maximum drain-to-source voltage, VDS(MAX), must be high enough to withstand the highest voltage seen in the application. Considering 35V as the maximum application voltage due to load dump, MOSFETs with VDS voltage rating of 40V is chosen for this application.
The maximum VGS TPS12000-Q1 can drive is 11V, so a MOSFET with 15V minimum VGS rating must be selected.
To reduce the MOSFET conduction losses, an appropriate RDS(ON) is preferred.
Based on the design requirements, BUK7J1R4-40H is selected and its ratings are:
40V VDS(MAX) and ±20V VGS(MAX)
RDS(ON) is 1.06mΩ typical at 10-V VGS
MOSFET Qg(total) is 73nC typical
TI recommends to make sure that the short-circuit conditions such max VIN and ISC are within SOA of selected FET (Q1) for at-least > tSC timing.
The internal charge pump charges the external bootstrap capacitor (connected between BST and SRC pins) with approximately 345μA. Use the following equation to calculate the minimum required value of the bootstrap capacitor for driving BUK7J1R4-40H MOSFET
Choose closest available standard value: 100nF, 10 %.
The RISCP sets the short-circuit protection threshold, whose value can be calculated using below equation:
To set 100A as short-circuit protection threshold, RISCP value is calculated to be 40.5kΩ.
Choose the closest available standard value: 40.2kΩ, 1%.
In case where large di/dt is involved, the system and layout parasitic inductances can generate large differential signal voltages between CS+ and CS- pins. This action can trigger false short-circuit protection and nuisance trips in the system. To overcome such scenario, TI suggests to add placeholder for RC filter components across sense resistor (RSNS) and tweak the values during test in the real system. The RC filter components should not be used in current sense designs by MOSFET VDS sensing to avoid impact on the short-circuit protection response.
For the design example under discussion, overcurrent transients are allowed for 50μs duration. This blanking interval, tSC (or circuit breaker interval, TCB) can be set by selecting appropriate capacitor CTMR from TMR pin to ground. The value of CTMR to set 50μs for tSC can be calculated using following equation:
Choose closest available standard value: 3.3nF, 10%.
The undervoltage lockout (UVLO) and overvoltage set point are adjusted using an external voltage divider network of R1, R2 and R3 connected between VS, EN/UVLO, OV and GND pins of the device. The values required for setting the undervoltage and overvoltage are calculated by solving Equation 12 and Equation 13.
For minimizing the input current drawn from the power supply, TI recommends to use higher values of resistance for R1, R2 and R3. However, leakage currents due to external active components connected to the resistor string can add error to these calculations. So, the resistor string current, I(R123) must be chosen to be 20 times greater than the leakage current of UVLO and OV pins.
From the device electrical specifications, V(OVR) = 1.24V and V(UVLOR) = 1.24V. From the design requirements, VINOVP is 36V and VINUVLO is 6.5V. To solve the equation, first choose the value of R1 = 470kΩ and use Equation 12 to solve for (R2 + R3) = 108.3kΩ. Use Equation 13 and value of (R2 + R3) to solve for R3 = 19.6kΩ and finally R2 = 88.7kΩ. Choose the closest standard 1 % resistor values: R1 = 470kΩ, R2 = 88.7kΩ, and R3 = 19.6kΩ.