SLVSFK0A May 2024 – August 2024 TPS22991
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The input to output voltage drop in the device is determined by the RON of the device and the load current. The RON of the device depends upon the VIN condition of the device. After the RON of the device is determined based upon the VIN condition, use the below equation to calculate the input to output voltage drop.
where
An appropriate ILOAD must be chosen such that the IMAX specification of the device is not violated.
To determine how much inrush current is caused by the load capacitance, use Equation 3.
The slew rate of the device dVOUT/dt at a given VIN voltage can be found in the electrical characteristic table for a given version. IINRUSH has to be within the IMAX and IPLS limits.