SLVSDX2A September 2017 – December 2017 TPS23521
PRODUCTION DATA.
The VDS threshold when the TPS23521 switches over from ICL1 to ICL2 (VD,SW) can be computed using Equation 1. For example, if a 15-V switch over is desired, RD should be set to 270 kΩ.