SLVSEI3C October 2018 – May 2020 TPS25982
PRODUCTION DATA.
The undervoltage lockout (UVLO) trip point is adjusted using the external voltage divider network of RVL1 and RVL2 connected between IN, EN/UVLO and GND pins of the device. The resistor values required for setting the undervoltage are calculated using Equation 13.
For minimizing the input current drawn from the power supply, TI recommends to use higher values of resistance for RVL1 and RVL2. However, leakage currents due to external active components connected to the resistor string can add error to these calculations. So, the resistor string current, IRVL12 must be 20 times greater than the leakage current (IENLKG).
From the device electrical specifications, UVLO rising threshold VUVLO(R) = 1.2 V. From design requirements, VINUVLO = 10.8 V. First choose the value of RVL1 = 1 MΩ and use Equation 13 to calculate RVL2 = 125 kΩ.
Use the closest standard 1% resistor values: RVL1 = 1 MΩ, and RVL2 = 125 kΩ