SLVSHR9 December 2024 TPS25984B
PRODUCTION DATA
The TPS25984Bx responds to output overcurrent conditions during steady-state by performing a circuit-breaker action after an internal transient fault blanking interval. This action allows the device to support a higher peak current for a short interval but also ensures robust protection in case of persistent output faults.
The device constantly senses the output load current and provides an analog current output (IILIM) on the ILIM pin which is proportional to the load current, which in turn produces a proportional voltage (VILIM) across the ILIM pin resistor (RILIM) as per Equation 28.
Where GILIM is the current monitor gain (IILIM : IOUT)
The overcurrent condition is detected by comparing this voltage against the voltage on the IREF pin as a reference. The reference voltage (VIREF) can be controlled in two ways, which sets the overcurrent protection threshold (IOCP) accordingly.
The overcurrent protection threshold during steady-state (IOCP) can be calculated using Equation 29.
Maintain VIREF within the recommended voltage range to ensure proper operation of the overcurrent detection circuit.
TI recommends to add a 150pF capacitor from IREF pin to GND for improved noise immunity.
After an overcurrent condition is detected, that is the load current exceeds the programmed current limit threshold (IOCP), but stays lower than the short-circuit threshold (2 × IOCP or IFFT whichever is lower), the device starts an internal blanking timer. If the load current drops below the current limit threshold before the timer expires, the circuit-breaker action is not engaged. This action allows transient load pulses to pass through the device without tripping the circuit. If the overcurrent condition persists for longer than the timer duration (tITIMER), the circuit-breaker action turns off the FET immediately.
Equation 8 can be used to calculate the RILIM value for the desired overcurrent threshold.
Figure 7-4 illustrates the overcurrent response for TPS25984Bx eFuse. After the part shuts down due to a circuit-breaker fault, it either stays latched off (TPS25984B2 variant with MODE pin floating or TPS25984B0/3 variants) or restarts automatically after a fixed delay (TPS25984B2 variant with MODE pin connected to GND or TPS25984B1 variant).