SLVSGG4B september 2022 – june 2023 TPS25990
PRODUCTION DATA
STATUS_WORD is a standard PMBus® command that returns two bytes of information with a summary of the eFuse fault conditions.
This command uses the PMBus® read word protocol.
To clear the bits in this register, the underlying faults must be removed and the CLEAR_FAULTS command must be issued by the host controller.The low byte of STATUS_WORD is the same register as the STATUS_BYTE command. The STATUS_WORD register contents are described in Figure 8-18 and Table 9-69.
Bit | Name | Value | Description | Default | Access |
---|---|---|---|---|---|
15 | OUT_STATUS | OUTPUT fault status | Read | ||
1 | Active bits set in the STATUS_OUT register | 0 | |||
0 | No active bits set in the STATUS_OUT register | ||||
14 | IOUT_STATUS | IOUT fault status | |||
1 | Active bits set in the STATUS_IOUT register | 0 | |||
0 | No active bits set in the STATUS_IOUT register | ||||
13 | INPUT_STATUS | INPUT fault status | |||
1 | Active bits set in the STATUS_INPUT register | 0 | |||
0 | No active bits set in the STATUS_INPUT register | ||||
12 | MFR_STATUS | Manufacturer specific fault status | |||
1 | Active bits set in the STATUS _MFR_SPECIFIC register | 0 | |||
0 | No active bits set in the STATUS _MFR_SPECIFIC register | ||||
11 | PGOODB | Power Good status | |||
1 | PGOOD de-asserted | 1 | |||
0 | PGOOD asserted | ||||
10:9 | Reserved | 00 | Reserved | 00 | |
8 | UNKNOWN | 1 | An event other than the ones listed in bits 15:1 has occurred | 0 | |
0 | An event other than the ones listed in bits 15:1 has not occurred | ||||
7:0 | Same as STATUS_BYTE register |
Figure 8-19 depicts the relationship between the STATUS_BYTE register, the STATUS_WORD register and the more detailed status registers.
Based on the information in these bytes, the host can get more insight by reading the appropriate status registers.