SLVSGY2 October 2023 TPS2HCS10-Q1
ADVANCE INFORMATION
Refer to the PDF data sheet for device specific package drawings
The TPS2HCS10-Q1 output channels are typically among a large number of channels in an ECU. The ECUs need to consume uAs of of current while the car is in park mode or key-off mode. The SLEEP mode is lowest current consumption mode of the IC with current consumption of the order of a uA per channel. In the key-off mode for the car, the TPS2HCS10-Q1 can be in either LPM mode when at least one channel has to supply a load ECU or in the SLEEP state where all the channels are OFF and the digital/ VDD circuits are all powered off. The SPI command as a write to the SLEEP register places the device in the SLEEP state. The VDD and VBB pins of the IC are expected to be powered in the SLEEP state.
In the SLEEP state the device is mostly powered off, so that the overall current consumption from VBAT of the ECU is minimized for a totality of the high-side switch channels. In this mode the a low nCS pin can wake up the device and place the device in the CONFIG state ready for SPI communication. However, SPI communication (actual data communication) can happen only after the tREADY period.