SNVSBI5A July 2019 – September 2019 TPS3870-Q1
PRODUCTION DATA.
The manual reset (MR) input allows a processor or other logic circuits to initiate a reset. A logic low on MR causes RESET to assert. After MR returns to a logic high and the SENSE pin voltage is within a valid condition (VSENSE < VIT+(OV)) , RESET is deasserted after the reset delay time (tD). If MR is not controlled externally, then MR can either be connected to VDD or left floating because the MR pin is internally pulled up to VDD. Figure Figure 19 shows the relation between MR and RESET.