SLUS593J December 2003 – June 2022 TPS40054 , TPS40055 , TPS40057
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The switching frequency is based on the minimum duty cycle ratio and the propagation delay of the current limit comparator. In order to maintain current limit capability, the on time of the upper MOSFET, tON, must be greater than 300 ns (see the Electrical Characteristics). Therefore:
Using 400 ns to provide margin,
Since the oscillator can vary by 10%, decrease fSW, by 10%
and, therefore, choose a frequency of 300 kHz.