SLUS930D April 2011 – November 2016 TPS40400
PRODUCTION DATA.
PIN | I/O(1) | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
ADDR0 | 21 | I | Low-order address pin for PMBus address configuration. One of eight resistor values must be connected from this pin to SGND to select the low-order octal digit in the PMBus address. |
ADDR1 | 22 | I | High-order address pin for PMBus address configuration. One of eight resistor values must be connected from this pin to SGND to select the high-order octal digit in the PMBus address. |
BOOT | 18 | I | Gate drive voltage for the high-side, N-channel MOSFET. A capacitor (100-nF) typical must be connected between this pin and SW. |
BP3 | 13 | O | Bypass pin for the internal regulator that supplies power to the internal controls of the device. Normal regulation voltage is 3.3 V. Connect a capacitor with a value of 100-nF or larger from this pin to GND. |
BP6 | 14 | O | Bypass pin for the internal regulator that supplies power to the gate drivers. Normal regulation voltage is 6.5 V. Connect a capacitor with a value of 1-μF or larger from this pin to GND. |
CLK | 1 | I | Clock input for the PMBus interface |
CNTL | 2 | I | Logic level input that controls the start-up and shutdown of the converter. PMBus options determine exact functionality. |
COMP | 6 | O | Output of the error amplifier. Used for control loop compensation. |
DATA | 24 | I/O | Data I/O for the PMBus interface |
DIFFO | 8 | O | Output of the unity gain remote voltage sense amplifier. Typically connected to the voltage divider on FB |
FB | 7 | I | Inverting input to the error amplifier. A voltage divider is connected to from the DIFFO pin to the FB pin to sense the output voltage. |
GND | 15 | – | Common connection for the device. This pin should connect to the thermal pad under the device package and to the power stage ground, preferably close to the source of the low-side or rectifier MOSFET. Connections should be arranged so that no high-power level currents flow across the pad connected to the thermal pad on the underside of the device. |
HDRV | 19 | O | Gate drive signal to the high-side MOSFET |
ISNS– | 11 | I | Inverting input to the current sense amplifier |
ISNS+ | 12 | I | Noninverting input to the current sense amplifier |
LDRV | 16 | O | Output used to drive the gate of the low-side or rectifier MOSFET. |
PGOOD | 3 | O | Power good output. This is an open-drain output that pulls low when any fault condition exists within the device or when the device is not operating within a user-selectable operating range of the nominal output voltage of the converter. |
SGND | PAD | – | Signal ground for the device. Connect the ground of signal level circuits to this pin. Connections should be arranged so that power level currents do not flow in the pad attached to the thermal plane or in the SGND portion of the circuit. |
SMBALRT | 23 | O | Output used to signal that PMBus host that the device needs attention. |
SW | 17 | I | This is the common connection for the flying high-side MOSFET driver and also serve as a sense line for the adaptive anti-cross-conduction circuitry |
SYNC | 4 | I | Logic level input to the oscillator inside the device. The oscillator resets on the rising edge of a pulse train applied to this pin and begin a new switching cycle. |
TRACK | 5 | I | Analog input to the noninverting side of the control loop error amplifier. The error amplifier has three inputs (voltage reference, TRACK and soft-start time) to its + side, and the lowest voltage applied to these three inputs dominate and control the output voltage of the whole converter. This pin is to allow the user to configure a voltage divider that allows the device output follow an external reference voltage during start-up. |
VDD | 20 | I | Input power connection for the device. This pin requires a supply voltage of between 3 V to 20 V. |
VSNS+ | 9 | I | Noninverting input to the unity gain remote voltage sense amplifier. |
VSNS– | 10 | I | Inverting input to the unity gain remote voltage sense amplifier. |