SLUSAQ4G October 2011 – September 2022 TPS40422
PRODUCTION DATA
The switching frequency is set by the value of the resistor connected from the RT pin to AGND. The RT resistor value is calculated in Equation 5.
where
When the TPS4022 device is synchronized to an external clock, the external clock frequency should be two times the free running frequency that is set by RT resistor. The variation of the external clock frequency should be within ±20%, and the switching frequency is one half of the actual clock frequency.