SLVSA38B December 2009 – July 2017 TPS43331-Q1
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPS43331-Q1 is a combination of two switched-mode, synchronous step-down controllers and two linearly-regulated power supplies. These devices are configured to drive external NMOS power switches and control the energy in the inductor by limiting the current using a resistor current sense feedback. The output voltage is regulated using an external resistor feedback network. The regulated output voltage can be programmed to a specified range using different feedback thresholds at the VFB(x) terminal. To minimize ripple current on the input line, the two buck regulators are switched 180º out of phase.
The protected high-side output is controlled by a discrete input to switch auxiliary input power to other devices in the system. The standby regulator VSTBY is enabled when the input power from the protected terminal of the battery supply is available to the device. The standby regulator consumes less than 75 μA, with less than 100 μA of load current on the regulated output terminal (VSTBY).
The calculations from the Buck Regulators section result in the schematic shown in Figure 20.
The design requirements for the switching regulator design in Figure 20 are listed in Table 3.
Assume Type III Compensation network for each buck regulator.
For this design example, use the parameters listed in Table 3.
The LC output filter gives a Double Pole which has a –180° phase shift.
The ESR of the output capacitor, CO, gives a zero that has a 90° phase shift.
The values of R1 and RS2 are chosen based on the desired VBUCK.
where
Use the following equations to select the resistor vales:
Select RS2 = 10 kΩ
where
The fc is typically 1/5 to 1/10 of the switching frequency.
Use Equation 8 to calculate the PWM modulator gain (K).
Use Equation 9 to calculate the amplifier gain (Av).
fc = fSW × 0.1 (the cutoff frequency when the gain is 1 is called the unity gain frequency).
The fc is typically 1/5 to 1/10 of the switching frequency double pole frequency response due to the LC output filter.
The LC output filter gives a Double Pole which has a –180° phase shift.
The ESR of the output capacitor, CO, gives a zero that has a 90° phase shift.
where
Use Equation 17 to calculate the PWM modulator gain (K).
where
Use Equation 18 to calculate the amplifier gain (Av).
Use the following guidelines for compensation components:
Make the two zeroes close to the double pole (LC); for example, fZ1 ≈ fZ2 ≈ 1 / 2π × (LCO)1/2.
Make the two poles above the cross-over frequency fc.
Use the following equations to select the resistor values:
Select RS2 = 10 kΩ
Calculate C1 based on placing a zero at 50% to 75% of the output filter double pole frequency.
Calculate C2 by placing the first pole at the ESR zero frequency.
Set the second pole at 0.5 the switching frequency and also set the second zero at the output filter double pole frequency.
Use Equation 30 to calculate and select the desired inductor ripple current (ΔIL).
where
The typical inductor ripple current is between 20% to 40% of the maximum output current.
Use Equation 31 to calculate the value of the inductor (L).
where
Use Equation 32 to calculate the value of the the rms and peak current flowing in the inductor is.
Use Equation 33 to calculate the inductor peak current.
Use Equation 34 to calculate the value of the output voltage ripple.
Usually the first term is dominant. The output ripple voltage is typically within the tolerance of the output specification.
Use Equation 35 to calculate the value of the output capacitor.
where
The difference between the maximum to minimum output current is the worst case load step in the system where:
VBUCK(max) is the maximum tolerance of the regulated output voltage.
VBUCK(min) is the minimum tolerance of the regulated output voltage.
The power dissipation is largely dependent on the MOSFET driver current and input voltage. The drive current is proportional to the total gate charge of the external MOSFET.
Assuming both high-side and low-side MOSFETs are identical in a synchronous configuration, use Equation 37 to calculate the total power dissipation.
The total power dissipation for the dual-channel controller is:
Use Equation 39 to calculate the device power consumption.
Use Equation 40 to calculate the power of the standby linear regulator.
Use Equation 41 to calculate the power of the linear regulator.
Use Equation 39 to calculate the power of the high-side driver.
Therefore, use Equation 43 to calculate the total power dissipation (PTotal).
Use Equation 31 to find the inductor value and assume an inductor ripple current of 0.8 A.
L = 20.2 µH, use a value of 22 µH
Use Equation 33 to calculate the peak inductor current (IL(peak)).
IL(peak) = 2.4 A
Use Equation 35 to calculate the output capacitance.
Assume a tolerance of ±3% to allow for some margin, the minimum IO current is 20 mA. Using Equation 34, the value of the minimum output capacitor, CO(min), is 29.3 µF. Considering temperature variations and manufacture tolerance, choose a value of 68 µF or greater for CO(min).
For this design, the value of CO is 100 µF.
Use Equation 14 to determine the double pole:
fLC = 3.39 kHz
Use Equation 15 to determine the zero due to the ESR of the output capacitor CO with ESR = 60 mΩ:
fESR = 26.5 kHz
fC = 0.08 × fSW = 20 kHz
Us Equation 24 and assume R27 = 10 kΩ to find the value of R23:
R23 = 40.2 kΩ
Use Equation 25 to find the value of R25:
R25 = 30.5 kΩ, Choose R25 = 29.4 kΩ
Use Equation 26 to find the value of C20:
C20 = 3.13 nF, Choose C20 = 3.3 nF
Use Equation 27 to find the value of C23:
C23 = 213 pF, Choose C23 = 220 pF
Us Equation 28 to find the value of R20:
R20 = 1.12 kΩ, Choose R20 = 1.1 kΩ
Use Equation 29 to find the value of C18:
C18 = 1142 pF, Choose C18 = 1200 pF
Using the same method for calculating the component values for Buck Regulator 2, with the set output conditions, the following values were selected.
Use Equation 31 to find the inductor value and assume an inductor ripple current of 0.3 A:
L = 19.2 µH, use a value of 22 µH
From Equation 33, the peak inductor current is:
IL(peak) = 1.65 A
Assume a tolerance of ±3% to allow for some margin and a minimum IO current of 20 mA. Use Equation 35 to calculate the value of the output capacitor:
CO(min) = 32.7 µF, with temperature variations and manufacture tolerance choose a value of 100 µF for this design.
CO = 100 µF
Use Equation 14 to determine the double pole:
fLC = 3.39 kHz
Use Equation 15 to determine the zero from the ESR of the output capacitor, CO, with ESR = 60 mΩ:
fESR = 26.5 kHz
fc = 0.8 × fSW = 20 kHz
Use Equation 24 and the R32 value of 17.4 kΩ:
R34 = 40.2 kΩ
Use Equation 25:
R33 = 30.3 kΩ, Choose R33 = 29.4 kΩ
Use Equation 26:
C26 = 3.129 nF, Choose C26 = 3.3 nF
Use Equation 27:
C29 = 213 pF, Choose C29 = 220 pF
Use Equation 28:
R35 = 1.1 kΩ , Choose R35 = 1.1 kΩ
Use Equation 29:
C27 = 1142 pF, Choose C27 = 1200 pF
Figure 40 shows an example of configuration for car-audio power-supply application. Other combinations are possible depending on the system requirements.