SLVSHN0 September 2024 TPS548B23
ADVANCE INFORMATION
The device requires input bypass capacitors between both pairs of VIN and PGND pins to bypass the power-stage. The bypass capacitors must be placed as close as possible to the pins of the IC as the layout allows. At least 20µF nominal of ceramic capacitance and two high frequency ceramic bypass capacitors are required. A 0.1μF to 1μF capacitor must be placed as close as possible to both VIN pins 4 and 12 on the same side of the board of the device to provide the required high frequency bypass, to reduce the high frequency overshoot and undershoot on across the power-stage on the VIN and SW pins. TI recommends at least 1μF of bypass capacitance as close as possible to each VIN pin to minimize the input voltage ripple. The ceramic capacitors must be a high-quality dielectric of X6S or better for the high capacitance-to-volume ratio and stable characteristics across temperature. In addition to this, more bulk capacitance can be needed on the input depending on the application to minimize variations on the input voltage during transient conditions.
The input capacitance required to meet a specific input ripple target can be calculated with Equation 21. A recommended target input voltage ripple is 5% the minimum input voltage, 780 mV in this example. The calculated input capacitance is 5.5μF. This example meets these two requirements with 2 × 10µF ceramic capacitors.
The capacitor must also have an RMS current rating greater than the maximum input RMS current in the application. The input RMS current the input capacitors must support is calculated by Equation 23 and is 12.4A in this example. The ceramic input capacitors have a current rating greater than this value.
For applications requiring bulk capacitance on the input, such as ones with low input voltage and high current, TI recommends the selection process in How to select input capacitors for a buck converter.