The TPS548D26 device
has an internal 4.5-V LDO featuring input from the AVIN pin and output to
the VCC pin. When the AVIN voltage rises, the internal LDO is
enabled automatically and starts regulating the LDO output voltage on the
VCC pin. The VCC voltage provides the bias voltage for the internal
analog circuitry on the controller side, and the VDRV voltage provides the supply
voltage for the power stage side.
Either the VCC or VDRV pin must be bypassed with a
2.2-μF, at least 6.3-V rating ceramic capacitor. Connecting the VCC pin decoupling
capacitor to AGND is required to provide a clean ground for the analog circuitry on
the controller side. Referring the VDRV pin decoupling capacitor to PGND is required
to minimize the parasitic loop inductance for the driver circuitry in the power
stage. Placing a 1-Ω resistor between the VCC pin and VDRV pin forms a RC filter on
VCC pin, which greatly reduces the noise impact from power stage driver circuit.
An external bias ranging from 4.75 V to 5.30 V can
be connected to the VDRV and VCC pin and power the IC. This action enhances
the efficiency of the converter because the VCC and VDRV power supply current now
runs off this external bias instead of the internal linear regulator.
A VDRV UVLO circuit monitors the VDRV pin
voltage and disables the switching when the VDRV voltage level falls below the VDRV
UVLO falling threshold. Maintaining a stable and clean VDRV voltage is
required for a smooth operation of the device.
Considerations when using an external bias on the
VDRV and VCC pin are shown below:
- Connect the external bias to
VDRV pin directly. Place a 1-Ω resistor between the VCC pin and VDRV pin,
then VCC is powered through the 1-Ω filtering resistor.
- For a configuration that the VCC pin and AVIN pin
are shorted together, the internal LDO is always forced off. A valid
external bias is required to be connected to VDRV pin (VCC pin and AVIN pin
are also powered by the same external bias through the 1-Ω filtering
resistor) so that the internal analog circuits have a stable power supply
rail at the power enable.
- For a configuration that the AVIN pin is not
shorted to VCC pin, when the external bias is applied on the VDRV pin
earlier than AVIN rail (VCC pin is also powered by the same external bias
through the 1-Ω filtering resistor), the internal LDO is always forced off
and the internal analog circuits have a stable power supply rail at the
power enable.
- The VCC and VDRV pins must be powered by the same source, either the
internal VCC LDO, or the same external bias.
- (Not recommended) When the external bias is applied on the VDRV pin late
(for example, after AVIN rail ramp-up), any power-up and power-down
sequencing can be applied as long as there is no excess current pulled out
of the VCC pin. Understand that an external discharge path on the VCC or
VDRV pin, which can pull a current higher than the current limit of the
internal LDO, can potentially turn off VCC LDO thereby shutting off the
converter output.
- A good configuration is:
Place a 1-Ω resistor between the VCC pin and VDRV pin, and shorting the AVIN
pin to VCC pin.
- A good power-up sequence with above configuration
is: the external 5-V bias is applied to VDRV pin first (VCC pin is also
powered by the same external bias through the 1-Ω filtering resistor), then
the 12-V bus applied on PVIN pin, and then the EN signal goes high.