SLVSGP3A May 2023 – February 2024 TPS54KB20
PRODUCTION DATA
The device requires input bypass capacitors between both pairs of VIN and PGND pins to bypass the power-stage. The bypass capacitors must be placed as close as possible to the pins of the IC as the layout allows. At least 20µF nominal of ceramic capacitance and two high frequency ceramic bypass capacitors are required. This device has a hard limit of 20µF. Some applications can require greater capacitance and can even require a bulk capacitor. Derating can impact the effective input capacitance value. A 0.1μF to 1μF capacitor must be placed as close as possible to both VIN pins 3 and 9 on the same side of the board of the device to provide the required high frequency bypass, to reduce the high frequency overshoot and undershoot across the power-stage from VIN to SW and SW to PGND. TI recommends at least 1μF of bypass capacitance as close as possible to each VIN pin to minimize the input voltage ripple. The ceramic capacitors must be a high-quality dielectric of X6S or better for the high capacitance-to-volume ratio and stable characteristics across temperature. In addition to this requirement, more bulk capacitance can be needed on the input depending on the application to minimize variations on the input voltage during transient conditions.
The input capacitance required to meet a specific input ripple target can be calculated with Equation 32. A recommended target input voltage ripple is 5% the minimum input voltage, 225mV in this example. The calculated input capacitance is 27.2μF and this meets the minimum input capacitance of 20µF.
The capacitor must also have an RMS current rating greater than the maximum input RMS current in the application. The input RMS current the input capacitors must support is calculated by Equation 34 and is 11.2A in this example. The ceramic input capacitors have a current rating greater than this value.
For applications requiring bulk capacitance on the input, such as ones with low input voltage and high current, TI recommends the selection process in How to select input capacitors for a buck converter analog design journal.