Before beginning a design using the device,
consider the following:
- Make VIN,
PGND, and SW traces as wide as possible to reduce trace impedance and improve heat
dissipation.
- Place the power components (including input and
output capacitors, the inductor, and the IC) on the top side of the PCB. To shield and
isolate the small signal traces from noisy power lines, insert at least one solid ground
inner plane.
- Make note that placement of the VIN decoupling
capacitors are important for the power MOSFET robustness. A 1μF/25V/0402 ceramic
high-frequency bypass capacitor on each VIN pin (pin 3 and 9) is required, connected to
the adjacent PGND pins (pin 4 and 8 respectively). Place the remaining ceramic input
capacitance next to these high frequency bypass capacitors. The remaining input
capacitance can be placed on the other side of the board, but use as many vias as
possible to minimize impedance between the capacitors and the pins of the IC.
- Place eight vias below the PGND pins (pins 4, 8,
and 16) and as many vias as possible near the PGND pins (pin 4 and 8). This action
minimizes parasitic impedance and also lowers thermal resistance.
- Use vias
near both VIN pins and provide a low impedance connection between them through an
internal layer. A via can also be placed below each of the VIN pins.
- Place the VCC decoupling capacitor as close as
possible to the device, with a short return to PGND pin 8. Make sure the VCC decoupling
loop is small and use traces with a width of 12 mil or wider to route the
connection.
- Place the BOOT capacitor as close as possible to
the BOOT and SW pins. Use traces with a width of 12
mil or wider to route the connection.
- Make the switch node as short and wide as
possible. The PCB trace, which connects the SW pin and high-voltage side of the
inductor, is defined as switch node.
- Always place the feedback
resistors near the device to minimize the FB trace distance, no matter
single-end sensing or remote sensing.
- For remote sensing, the connections from the FB
voltage divider resistors to the remote location must be a differential pair of PCB
traces, and must implement Kelvin sensing across a bypass capacitor of 0.1μF or
higher. The ground connection of the remote sensing signal must be connected to
GOSNS pin. The VOUT connection of the remote sensing signal must be
connected to the feedback resistor divider with the bottom feedback resistor
terminated to the GOSNS pin. To maintain stable output voltage and minimize the
ripple, the pair of remote sensing lines must stay away from any noise sources such
as inductor and SW nodes, or high frequency clock lines. TI recommends to shield the
pair of remote sensing lines with ground planes above and below.
- For single-end sensing, connect the top feedback
resistor between the FB pin and the output voltage to a high-frequency local output
bypass capacitor of 0.1μF or higher, and short GOSNS to AGND with a short
trace.
- Connect
the AGND pin (pin 2) to the PGND pad (pin 16)
beneath the device.
- Return
the MSEL resistor, ILIM resistor, and SS capacitor to a quiet AGND island.
- Avoid routing the PG signal and any
other noisy signals in the application near noise sensitive signals, such as ILIM, FB
and GOSNS to limit coupling.
- See Layout Example for the layout recommendation.