SLVS939B June 2009 – December 2014 TPS55332-Q1
PRODUCTION DATA.
The TPS55332-Q1 device is designed to operate from an input voltage up to 40 V. Ensure that the input supply is well regulated. Furthermore, if the supply voltage in the application is likely to reach negative voltage (for example, reverse battery) a forward diode must be placed at the input of the supply. For the VIN pin, a small ceramic capacitor with a typical value of 0.1μF is recommended. Capacitance de-rating for aging, temperature, and DC bias must be taken into account while determining the capacitor value. Connect a local decoupling capacitor close to the BOOT pin for proper gate drive voltage for the internal MOSFET switch.