SLVS431C june 2002 – September 2015 TPS61130 , TPS61131
PRODUCTION DATA.
For all switching power supplies, the layout is an important step in the design, especially at high peak currents and high switching frequencies. If the layout is not carefully done, the regulator could show stability problems as well as EMI problems. Therefore, use wide and short traces for the main current path and for the power ground tracks. The input capacitor, output capacitor, and the inductor must be placed as close as possible to the device. Use a common ground node for power ground and a different one for control ground to minimize the effects of ground noise. Connect these ground nodes at any place close to one of the ground pins of the device.
The feedback divider must be placed as close as possible to the control ground pin of the device. To lay out the control ground, TI recommends using short traces as well, separated from the power ground traces. This avoids ground shift problems, which can occur due to superimposition of power ground current and control ground current.
Implementation of integrated circuits in low-profile and fine-pitch surface-mount packages typically requires special attention to power dissipation. Many system-dependent issues such as thermal coupling, airflow, added heat sinks and convection surfaces, and the presence of other heat-generating components affect the power-dissipation limits of a given component.
Follow these three basic approaches for enhancing thermal performance.
The maximum recommended junction temperature (TJ) of the TPS6113x devices is 150°C. The thermal resistance of the 16-pin TSSOP package (PW) is RΘJA = 100.5 °C/W. The 16-pin VQFN package (RSA) with exposed thermal pad has a thermal resistance of RΘJA = 33.9°C/W, if the thermal pad is soldered and the board layout is optimized. Specified regulator operation is assured to a maximum ambient temperature TA of 85°C. Therefore, the maximum power dissipation is about 647 mW for the TSSOP (PW) package and 1917 mW for the VQFN (RSA) package. More power can be dissipated if the maximum ambient temperature of the application is lower (see Equation 11).
If designing for a lower junction temperature of 125°C, which TI recommends, maximum heat dissipation is lower. Using the above Equation 11 results in 1917-mW power dissipation for the RSA package and 647 mW for the PW package.