SLVSDA7E February 2017 – August 2019 TPS61178
PRODUCTION DATA.
The TPS61178x features of a wide adjustable switching frequency ranging up to 2.2 MHz. The switching frequency is set by a resistor connecting with the FREQ / SYNC pin. This pin cannot be left floating in the application. Use Equation 2 and Equation 3 to calculate the resistor value for a desired frequency.
where
For instance, if the RFREQ is 342 kΩ, the frequency is 500 kHz.
Figure 21 shows the switching frequency versus the setting resistor, which is measured with VOUT = 16 V from VIN = 7.2 V .