SLVSGS9G March 2023 – October 2025 TPS61299
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The TPS61299x/xA employs the input average current protection (OCP) function. If the inductor average current reaches the current limit threshold ILIM, the control loop can limit the inductor average current. In this case the output voltage decreases until the power balance between input and output is achieved. If the output drops below the input voltage, the TPS61299x/xA enters into Down Mode. If the output drops below 1.6V, the TPS61299x/xA enters into startup process again. In Pass-Through operation, input current limit function is not enabled.