The TPS61378-Q1 is designed to operate from
an input voltage supply range between 2.3 V to 14 V. This input supply must be well
regulated. If the input supply is located more than a few inches from the device, the
bulk capacitance can be required in addition to the ceramic bypass capacitors. An
electrolytic capacitor with a value of 47 µF is a typical choice.