SGLS118E December 2001 – July 2024 TPS769-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The adjustable-version device requires external feedback divider resistors to set the output voltage. VOUT is set using the feedback divider resistors, R1 and R2, according to the following equation:
where:
To ignore the FB pin current error term in the VOUT equation, set the feedback divider current to 100 times the FB pin current. This current is listed in the Electrical Characteristics table. This setting provides the maximum feedback divider series resistance, as shown in the following equation:
In Table 7-1, examples of R1 and R2 values are given for different output voltage options with a feedback divider current designed at 7μA.