SBVS343A March 2019 – September 2019 TPS7A78
PRODUCTION DATA.
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | SC1– | — | Negative terminal of the switched-capacitor, voltage-reduction stage pin. Connect a minimum 1-µF, X5R (or better) dielectric, 16-V-rated capacitor between this pin and the SC1+ pin. Place the capacitor as close to the device as possible; see the Recommended Operating Conditions table for details. |
2 | SC1+ | — | Positive terminal of the switched-capacitor, voltage-reduction stage pin. Connect a minimum 1-µF, X5R (or better) dielectric, 16-V-rated capacitor between this pin and the SC1– pin. Place the capacitor as close to the device as possible; see the Recommended Operating Conditions table for details. |
3 | SCIN | — | Rectified DC-voltage pin. Place the capacitor as close to the device as possible; see the Device Functional Modes section for the dual-input power-supply capability and the Calculating the Bulk Capacitor section for the proper capacitor calculation. |
4 | PFD | Input | Power-failure detect pin. An analog voltage input compares the reference voltage to a resistor-divided VSCIN voltage to detect a VAC power-failure; see the Recommended Operating Conditions table and the Calculating the PFD Pin Resistor Dividers for Power-Fail Detection section for details. |
5 | AC+ | Power | AC-supply line or neutral input to the device after the capacitive-drop (cap-drop) capacitor and surge resistor. Either this pin or the AC– pin must have the cap-drop capacitor and surge resistor in series with the line. See the Full-Bridge (FB) and Half-Bridge (HB) Configurations section for details. |
6 | GND | Ground | Ground pin. All device ground pins must be referenced to the same ground. Connect this pin to the thermal pad at the bottom of the device; see the Layout section for details. |
7 | AC– | Power | AC-supply line or neutral input to the device pin after the cap-drop capacitor and surge resistor. Either this pin or the AC+ pin must have the cap-drop capacitor and surge resistor in series with the line. See the Full-Bridge (FB) and Half-Bridge (HB) Configurations section for details. |
8 | LDO_OUT | Output | Regulated DC output pin. Connect a minimum 0.68-µF, X5R (or better) dielectric capacitor between this pin and the device GND pins. Place the capacitor as close to the device as possible; see the Recommended Operating Conditions table for the maximum capacitor value. |
9 | LDO_IN | — | Charge-pump output pin. Connect a minimum 0.68-µF, X5R (or better) dielectric capacitor between this pin and the device GND pins. This pin is internally driven and must not be driven externally. For optimal performance, connect a capacitor that is 10x the value of CLDO_OUT placed as close to the device as possible. See the Recommended Operating Conditions table for the maximum capacitor value. |
10 | PF | Output | Power-fail indicator pin. An open-drain indicator signal indicates if the VAC supply has failed. Pullup this pin through an external resistor to VLDO_IN or to a DC-rail that shares the same GND as the device. The PF pin goes low when VPFD is less than the VIT(PFD,FALLING) threshold, as specified in the Electrical Characteristics table. See the Recommended Operating Conditions table for proper selection of the pullup resistor. |
11 | PG | Output | Power-good indication pin. An open-drain indicator signal indicates if the VLDO_OUT surpassed the VIT(PG,RISING) threshold, as specified in the Electrical Characteristics table. Pullup this pin through an external resistor to VLDO_OUT or to a DC rail that shares the same GND as the device. See the Recommended Operating Conditions table for proper selection of the pullup resistor. |
12 | GND | Ground | Ground pin. All device ground pins must be referenced to the same ground. Connect this pin to the thermal pad at the bottom of the device; see the Layout section for details. |
13 | SC2+ | — | Positive terminal of the switched-capacitor, voltage-reduction stage pin. Connect a minimum 1-µF, X5R (or a better) dielectric, 10-V-rated capacitor between this pin and the SC2– pin. Place the capacitor as close to the device as possible; see the Recommended Operating Conditions table for details. |
14 | SC2– | — | Negative terminal of the switched-capacitor, voltage-reduction stage pin. Connect a minimum 1-µF, X5R (or a better) dielectric, 10-V-rated capacitor between this pin and the SC2+ pin. Place the capacitor as close to the device as possible; see the Recommended Operating Conditions table for details. |
Thermal pad | — | Exposed pad of the package. Connect this pad to device ground pins. Connect the thermal pad to a large-area ground plane for best thermal performance. |