SLVSFT8F February 2023 – December 2023 TPS7H1111-SEP , TPS7H1111-SP
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The PSRR (power supply rejection ratio) of the TPS7H1111, is the amount it attenuates the input noise at VIN, to the output, VOUT. It is mathematically defined in Equation 12.
The input noise is generally dominated by the switching ripple of an upstream converter. This noise occurs at the switching frequency and its harmonics.
The PSRR values are reported under various conditions and at different frequencies in both the Electrical Characteristics and the Typical Characteristics Figure 6-1 through Figure 6-11 . The TPS7H1111 is designed to have excellent PSRR across a wide variety of conditions. In order to further improve PSRR, operating conditions can be fine tuned. In general, the TPS7H1111 PSRR is most improved by the following (in relative order of importance):
PSRR is only minimally improved on the TPS7H1111 by the following:
The TPS7H1111 architecture is optimized for high PSRR due to its high loop bandwidth. In order to keep the bandwidth high, the output capacitance should be within the recommended operating conditions. Traditional techniques to improved PSRR by increasing output capacitance are not valid. This is because additional capacitance could reduce the loop bandwidth of the TPS7H1111. This reduced bandwidth will degrade PSRR more than the capacitance helps.
If additional PSRR at high frequency (for example, > 10 MHz) is desired, a ferrite bead may be utilized. The ferrite bead should be placed outside the TPS7H1111 control loop as shown in Section 9.2.1 as to not degrade the loop bandwidth or stability.
In addition to the PSRR from VIN to VOUT, PSRR is specified from VBIAS to VOUT as PSRRBIAS. It is defined in Equation 13.
Since the BIAS supply is relatively low current, an RC filter can be inserted between the BIAS supply and BIAS pin (typically 10 Ω and 4.7 μF) to increase the PSRRBIAS. The RC filter, combined with the internal ripple rejection of the internal bias regulator, provides very high PSRRBIAS as shown in Figure 6-13. Therefore, at typical switching frequencies between 100 kHz and 1 MHz (where high ripple rejection is the most important to filter the input ripple), PSRRBIAS remains very high to avoid becoming a major limiting factor in overall device PSRR. If an RC filter is unable to be utilized, the PSRRBIAS values will be degraded as shown in Figure 6-12.
If the bias supply is exceptionally noisy or if an RC filter is unable to be utilized, it may be beneficial to calculate the total output ripple coming from the input ripple on both the VIN and VBIAS supplies. The total output ripple is the superposition of the VIN ripple attenuated by its PSRR and the VBIAS ripple attenuated by its PSRRBIAS as shown in Equation 14. Note however that each term is frequency dependent.