SBVS445A October 2024 – December 2024 TPS7N53
PRODUCTION DATA
The TPS7N53 has an SS pin and an NR pin to independently control the soft-start time and reducing the noise generated by the internal band-gap reference and the external resistor RREF.
The device features a programmable, monotonic, voltage-controlled, soft-start circuit that is set to work with an external capacitor (CSS). In addition to the soft-start feature, the CNR capacitor lowers the output voltage noise of the LDO. The soft-start feature can be used to eliminate power-up initialization problems. The controlled output voltage ramp also reduces peak inrush current during start up, minimizing start-up transients to the input power bus.
To achieve a monotonic start up, the device output voltage tracks the VNR reference voltage until this reference reaches the set value (the set output voltage). The VNR reference voltage is set by the RREF resistor and, during start up, the device uses a fast charging current (ISS), as shown in Figure 7-2, to charge the CSS capacitor.
The 30μA (typical) ISS current quickly charges CSS until the voltage reaches approximately 90% of the set output voltage, then the ISS current turns off, the switch between NR and SS closes, as well as the switch between NR and REF.
The soft-start ramp time depends on the fast start-up (ISS) charging current, the reference current (IREF), CSS capacitor value, and the targeted output voltage (VOUT(target)). Equation 4 calculates the soft-start ramp time.
The ISS current is provided in the Section 5.5 and has a value of 30μA (typical). The IREF current has a value of 150μA (typical). The remaining 10% of the start-up time is determined by the RREF × CNR time constant.
The output voltage noise can be lowered significantly by increasing the CNR capacitor. The CNR capacitor and RREF resistor form a low-pass filter (LPF) that filters out noise from the VREF voltage reference, thereby reducing the device noise floor. The LPF is a single-pole filter and Equation 5 calculates the LPF cutoff frequency. Increasing the CNR capacitor can significantly lower output voltage noise. For low-noise applications, use a 1μF or larger CNR for optimal noise.
Figure 7-3 shows the impact of the CNR capacitor on the LDO output voltage noise.